HyperLynx screen shot of advanced PCB solvers.

Advanced Solvers

HyperLynx Advanced Solvers (HLAS) are a complete family of Electromagnetic (EM) simulation tools for PCB and IC packaging applications. They provide full-wave, hybrid and quasi-static simulation that can run standalone or as a tightly integrated part of Signal and Power Integrity analysis flows.

EM solver applications

Different applications require different EM modeling approaches to keep simulation times and resource requirements within reasonable limits. The correct solver to use for a job is determined based on the size of the structure to be modeled and the wavelengths of the frequencies of interest (FOI) in the structure.

When the structure is small (typically < 1/10 wavelength) next to the FOI, it can be considered as a "lumped" structure and a quasi-static analysis will suffice, which analyzes the structure both at DC and a single frequency point. This type of analysis is typical for extracting analog circuit parasitics at 10's of MHz and is also often suitable for small IC packages operating at moderate speeds.

When the structure is large, planar and regular, and frequencies are moderate (up to a few GHz), the hybrid technique decomposes the structure into planes and transmission lines, connected by vias. This approach is common for DDR analysis, where it's important to include the effects of non-ideal return paths in the interconnect model.

When frequencies are high (typically >5 GHz) and accuracy is critical, the full-wave approach is used, because it models the structure in the greatest detail and makes the fewest assumptions. This approach provides the most accurate results, but is also the most memory and compute-intensive. Parallel simulation techniques are often used to break the overall task into pieces that are run simultaneously to reduce the time required to complete the job.

HyperLynx Advanced Solvers provides all three simulation capabilities within a common framework, with the same database import and editing capabilities and with a common set of post-processing, visualization and model export tools. Once you've imported a design, you can switch solvers with the click of a button, depending on your output format and accuracy requirements.

HyperLynx integration and ease of use

3D electromagnetic simulation is a critical technology by itself, but it's also part of a larger analytical process that determines whether a system has enough positive operating margin to function reliably. Analyzing an individual structure allows it to be understood and optimized for electrical behaviors like insertion loss and crosstalk, but it's the behavior of the overall system that ultimately matters, not its individual elements.

HyperLynx Advanced Solvers are tightly integrated with HyperLynx Signal Integrity and HyperLynx Power Integrity flows to provide accurate, automated interconnect modeling as part of a system-level analysis workflow. This allows DDR interface, high-speed serial channel and AC power integrity analyses to be performed with the highest levels of modeling accuracy. PCB models are extracted and solved automatically as part of these system-level workflows.

With HyperLynx, the analysis flows have already been established, proven and documented - providing a ready to use flow right "out of the box”, or a baseline to build from when creating your own customized flows. HyperLynx Advanced Solvers can post-process data and output simulation results in a wide variety of different output formats to meet your particular needs.

HyperLynx screen shot showing the interface for Advanced Solvers integration with signal integrity and power integrity.

Scalable performance

3D electromagnetic simulation is a compute and memory-intensive task, with resource requirements that increase dramatically as structure size and modeling accuracy go up. HyperLynx Advance Solvers (HL-AS) let you scale solver performance two ways -by adding more CPU cores and by distributing large simulation runs across multiple machines. HL-AS Job Distribution (HL-AS JD) lets you split large jobs and run them in parallel across your LAN. Job Distribution includes a built-in job manager that allows HyperLynx to distribute simulation runs directly and is also compatible with popular load management systems.

Advanced design optimization

HyperLynx Advanced Solvers provides two levels of automated design optimization, which let users quickly determine which design modifications will result in optimum design performance. For each level, users define the structure to be optimized, the design parameters that can be modified and their ranges, along with the metrics used to measure design performance and target values.

  • HyperLynx 3D Explorer (3DEX) performs automated swept-parameter analysis on parameterized design templates that include BGA breakouts, cables, single-ended/differential traces and single-ended/differential vias. Portions of an actual, routed design can be extracted, parameterized and optimized. 3DEX normally generates simulation cases for all combinations of input design variables; the cases that are actually simulated can be selected by the user if the number of permutations gets too large. 3DEX is best suited to applications where the number of permutations is <100, or when the subset of cases that should be simulated can be readily identified.
  • HyperLynx Design Space Exploration (DSE) excels where the design space to be explored is very large (>100,000 permutations or more) and swept-parameter analysis is impractical. DSE is based on HEEDS-MDO, a powerful general-purpose optimization suite with comprehensive modeling, fitting and results visualization capabilities. DSE is extremely efficient - its advanced SHERPA algorithm can often investigate a 100,000 permutation design space and find a workable solution by running as few as 100 automatically selected simulation experiments.
HyperLynx visual interface with design optimization showing the 3D explorer.

Products